Skip to main content

InstaSeal® Technology Set to Revolutionize Fire Sprinkler Installation by Completely Eliminating Wrenches and Sealants

InstaSeal

Caledonia, Michigan - In an exciting development for the fire sprinkler industry, InstaSeal® technology(opens in a new window) is poised to transform the world of fire sprinkler installation. The InstaSeal family, which centers around a gasketed welded pipe outlet and the innovative "Torque-Assist" protective sprinkler cap, promises to streamline the installation process for sprinkler fitters across the industry.

The InstaSeal gasket seals the connection upon sprinkler installation and eliminates the need for sealants like PTFE tape or thread sealant that is typically used for sprinkler installation. The innovation of the integrity cap protects the rubber gasket once inserted inside the fitting.

James Golinveaux, CEO of Viking Group, Inc., expressed his excitement about this game-changing technology, stating, "InstaSeal technology represents a significant leap forward in fire sprinkler installation. Our goal was to simplify the process, eliminate the need for messy sealants and tape and empower contractors to tighten sprinklers by hand. We believe InstaSeal will revolutionize the way contractors work, saving them time and money."

This innovative offering provides a range of benefits, including simplifying the installation process by eliminating the need for sealants. The "Torque-Assist" protective cap enables effortless hand-tightening, removing the necessity for wrenches. InstaSeal not only streamlines workflows but also saves time and money, with faster installations and reduced labor costs. 

The InstaSeal welded outlet(opens in a new window) is precisely engineered to ensure dependable, leak-free seals. cULus Listed and FM Approved, the outlets have undergone extensive quality testing to ensure they meet the highest standards of performance and dependability when used alongside Viking sprinklers(opens in a new window)

Select Viking sprinklers are compatible with the advanced InstaSeal® technology through the addition of new "Torque-Assist" caps. Make sure to look for the compatibility icon to ensure the correct sprinklers are being ordered for a job requiring InstaSeal technology.

The available pipe sizes for a 1” and ¾” threaded fitting are 2”, 2.5” and 3”, with Schedule 10, 30, and 40 and Bull Moose Eddy Flow and Wheatland MegaFlow as the available pipe types. InstaSeal welded outlets have a maximum rated pressure of 175 psi (12 bar). You can find this novel InstaSeal technology at one of our Viking SupplyNet fabrication and distribution centers(opens in a new window).

InstaSeal is a pioneer in fire sprinkler installation technology, committed to simplifying the installation process and improving efficiency for contractors. With innovative solutions like the gasketed welded outlet and "Torque-Assist" protective cap, InstaSeal is at the forefront of the industry, providing contractors with cutting-edge technology set to redefine the industry.

 

Viking is a global leader in manufacturing and distributing innovative fire protection and life safety systems. For more than 100 years, the company’s products and services have protected lives and property worldwide from the devastating effects of fire. For more information on Viking’s complete line of fire protection products and services, visit www.vikinggroupinc.com.